|
|
|
|
|
Gates is the only manufacturer approved by virtually every major OEM to provide timing belts for new engines.
This means that Gates is able to cover the aftermarket with timing belts that are OE-equivalent or better in service life and performance.
Gates also has the largest selection of timing component kits for the aftermarket, with 75 percent of its kits being specified for import vehicles. Each kit for 1974 - 2004 model years contains all the parts needed for a timing belt system replacement: one or more timing belts, idlers and/or tensioners, and detailed instructions.
|
|
Timing Belt Replacement Guide
Timing belt replacement intervals for all major autmobile makes and models.
When the automaker doesn't make a specific recommendation, Gates suggests changing the timing belt at 60,000 miles.

|
| |
| |
Exact Fit for Imports
|
| |
Gates has the largest coverage for import engine applications ranging from Acura to Yugo vehicles.
|
| |
OE-Match timing belts  |
| |
 |
|
|
|
|
|
Interference Engine Issues
Got an Interference Engine?
Find Out Now
Timing belt-equipped car engines can be classified as either free-running or interference, depending on what occurs if piston/valve synchronization is lost due to a failed timing belt. As illustrated below, an interference engine usually sustains damage if synchronization is lost. This could result in very expensive engine repairs.

No Valve/Piston Interference

Valve/Piston Interference
Notes: Timing belt failure on interference engines can result in serious engine damage. See manufacturer's maintenance manual for specific information. Belts of similar dimensions and tooth profiles are not interchangeable due to varying construction features. Misapplication of belts voids manufacturer's warranty.
|
|
|
Timing Component Kits - Belt, Idler and Tensioner pulley
|
In the aftermarket, "job comebacks" are one of the biggest concerns for installers. They greatly reduce productivity and profitability, not to mention the loss of repeat business and negative word of mouth.
In the case of the timing belt system, Gates Rubber Company engineers have determined that belt failure "comebacks" are often caused by a faulty timing belt idler or tensioner pulley.
Gates line of Timing Component Kits allow you to service the complete timing system - including the belt(s), idler(s), tensioner pulley(s) and installation instructions.
|

|
Timing Component Kits
Note: Order Timing Component Kits and Oil Seals at the same time for less frustration.
Oil Seals - Ensure Maximum Timing Belt Life
|
To help installers do a complete job of replacing the timing belt drive system, Gates has a line of cam and crankshaft oil seals.
The seals will prevent oil contamination to a newly installed timing belt assembly, ensure maximum belt life and reduce costly "comebacks" that may result from future leaks at the cam and crankshaft.
Gates engineers recommend that installers replace these oil seals whenever they install Timing Component Kits to ensure the best replacement service and maximum customer satisfaction.
Oil Seals Info & list of Applications 
|

|
More than two-dozen oil seal kits for domestic and import cars are available from Gates. Each kit contains one, two or three seals, depending on the application.
Water Pumps
|
Gates is the most preferred and trusted supplier of cooling system belts and hoses.
Gates now offers you a line of new – not remanufactured – water pumps, designed and built for long lasting, efficient cooling.
Water Pumps 
|
 |
|
|
|
| |
|
|
|
|